AXIS#.WS.TSTANDSTILL

Description

In Wake & Shake mode 1, a maximum current of AXIS#.WS.IMAX is applied to the AXIS#.MOTOR. AXIS#.WS.TSTANDSTILL defines a wait time, during which this maximum current is held, before detecting the commutation angle of the AXIS#.MOTOR. Longer times are useful for big inertia motors or heavy loads.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

100 to 20,000

Default Value

5000
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
AXIS1.WS.TSTANDSTILL

5013h

12h

Unsigned16

-

-

Read/Write

No

AXIS2.WS.TSTANDSTILL

5113h

12h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.TSTANDSTILL

6717

1A3D

Unsigned16

Read/Write

-

AXIS2.WS.TSTANDSTILL

72253

11A3

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.TSTANDSTILL

6717

Unsigned16

Read/Write

-